Envelope Signal Generator

This block is to configure the Envelope Signal Generator instrument.

Instrument Connection Button

This button connects to the instrument after entering the its Address in the Configuration property grid. It also displays the following status conditions:

Configuration

Three types of instruments are supported in N7614B Signal Studio for Power Amplifier Test as Envelope Signal Generator.